Erwan Y

SPC5Studio 5.3.2 is available

Discussion created by Erwan Y Employee on Jun 6, 2017

Dear All ,

 

SPC5Studio 5.3.2 is available

 

*** Highlights ***

Here are the changes coming with SPC5Studio v5.3.2

- Serial Read not fully working in Linflex_v1 driver

 

Here are the changes coming with SPC5Studio v5.3.1

- Update the max values of K2 clockpoints

- Update Velvety Header File

- SPC560p.h header file issue: MDIS bit missing in the definition of MCR register in PIT tag

- Write one to clear (w1c) register issue

- Pinmap for BGA: allow flip of image to see device in order to have A1 ball in top left corner

 

- Several bugs and improvements, please refer to 

SPC5 Automotive MCUs (SPC5Studio part)

 

*** Notes ***
- Make sure to read the SPC5Studio Users Guide and Components
Writers Guide in
the help section.
Enjoy SPC5Studio,
The SPC5Studio Team.

Outcomes