AnsweredAssumed Answered

X-NUCLEO.IDW04A stuck in reset

Question asked by panduro.soeren.002 on Jun 7, 2017
Latest reply on Jun 7, 2017 by Mridupawan Das

HI 

 

We are planing to use a new WIFI module from ST for replacing the old module ( form another supplier )  

so I :

1. bought a NUCLEO-F401RE and a X-NUCLEO.IDW04A boards.

2. downloaded the en.x-cube-wifi1_firmware software. 

3. done the board setup according to page 6 in UM2183 (Getting started with the X-NUCLEO-IDW04A1)

4. compiled the firmware (Server_Socket) with IAR, and downloaded it to the board.

5. run.

 

and now the software get stuck in the wifi_reset() function wating for the stage to get started.

 

while(IO_status_flag.WiFi_WIND_State != WiFiHWStarted)
{
__NOP(); //nothing to do

 

so before I get started with the big investigation, I was thinking that maybe I wasn't the only one that have see this problem.

 

So I'm hoping that one of you guys can give me a hint, thanks in advance..

Outcomes