AnsweredAssumed Answered

LSM6DSL: Using inactivity interrupt without the auto-decrease of the sample rate

Question asked by Omnia . on Jun 5, 2017
Latest reply on Jun 6, 2017 by Miroslav B

Hi,

I am using the LSM6DSL with a SMT32L476. My question is in relation to the Sleep/inactivity interrupt.

I am able to use the LSM6DSL in both sleep and wake up interruption.

However is it possible to use this interrupt (Sleep/inactivity) and disable the automatic decrease of the accelerometer sampling rate to 13 Hz option.

 

I tried to set TAP_CFG (58h) to 0x80 (INACT_EN = b00) but the interrupts are not generated anymore.

 

Can someone please tell me if it is possible and if it is how to ?

 

Thanks,

Outcomes