AnsweredAssumed Answered

TFT Display using NUCLEO-F746ZG

Question asked by Ray Mendoza on May 31, 2017
Latest reply on Sep 8, 2017 by Dan Mackie

Hello!

 

I am a beginner using the the NUCLEO-F746ZG to drive a 4.3" Newhaven TFT display that has a capacitive touch panel controller.

 

The parts are shown below:

NUCLEO-F746ZG STMicroelectronics | Development Boards, Kits, Programmers | DigiKey

NHD-4.3-480272EF-ATXL#-CTP Newhaven Display Intl | Optoelectronics | DigiKey 

 

I was wondering if there is an example test code to see if the connections I made between the display and the nucleo are correct? I made my connections based on pins that can use the LTDC interface as an alternate function.

 

More info: I wish to pull images from an SD card. Certain pictures will be displayed depending on where the the user presses on the screen.

 

Thank you for the help!

Outcomes