AnsweredAssumed Answered

Request for enhancement : Cube 4.21.0

Question asked by Andrei Chichak on May 30, 2017
Latest reply on May 30, 2017 by Imen D
Branched from an earlier discussion

Eric,

 

In the implementation that was included in 4.21 there was a couple of MISRA violations inserted.

 

Unlike the assert_failed routine, _Error_Handler uses char* and int for parameters instead of uint8_t* and uint32_t.

 

Just a head-up.

 

Also, the USER CODE BEGIN and USER CODE END comments have an incorrect function name.

 

Andrei

Outcomes