AnsweredAssumed Answered

STM32F7 Disco USB3320

Question asked by Vitalii Mitko on May 26, 2017

STM32F7 Disco. I'm using the cube and keil.
So I got to HS, start with simple VCP, on FS USB it is correctly defined (after I removed VBUS sensing).
I generate the same empty project only for 2.0, on board the USB3320, the pins all match (in the cube I used not the choice of the chip but the choice of the board), VBUS tried both versions, the PC does not see the device.
Who raised this interface can tell you where to include or how to generate the code correctly?
P.s. The jumpers on the feeder are correct.

Attachments

Outcomes