AnsweredAssumed Answered

Is it possible to send AT command from a Nucleo-L0x to a B-L072Z board? (LoRa)

Question asked by maxence forget on May 26, 2017
Latest reply on Dec 19, 2017 by Andrew Neil

Hi,

 

My purpose is to realise a new set up for LoRa.

 

Before, I used a B-L072Z-LRWAN1 board with the I-CUBE-LRWAN1 software with the End Node code or the AT SLAVE code.

 

For the AT_SLAVE code, I used a terminal to send AT COMMAND to the MCU of my LoRa module.

 

Now, I want to configure my B-L072Z board with the AT_SLAVE code (as I realized before) but send AT_COMMAND with a Nucleo_L073RZ board with the AT_MASTER code (and not with a terminal). In comparison with this picture, I don't have application module and my AT_master module will be a the Nucleo_L073RZ board.

 

 

Is it possible? Is the AT_MASTER code functionnal with a Murata LoRa module? Should I just connect Tx-> Rx and Rx_>Tx and GND of the two board to communicate (UART) or there is some modification with jumper?

 

Thanks in advance!

Max

Outcomes