1 Reply Latest reply on May 19, 2017 9:01 PM by Dilbert K

    BlueMicrosystem2_V2.2.0 build with SystemWorkbench

    Dilbert K

      I just downloaded the BlueMicrosystem2_V2.2.0 and build with AC6 (System Workbench).

      The project I trying is :

      BlueMicrosystem2_V2.2.0\Projects\Multi\Applications\BlueMicrosystem2\SW4STM32\STM32L476RG-SensorTile\STM32L4xx-SensorTile

      What I have noticed is following :

      #ifdef STM32_NUCLEO
      0x80,
      #elif STM32_SENSORTILE
      0x02,
      #endif /* STM32_NUCLEO */

      My understanding in gcc, "#elif" would not be supported.  Since the project is using the Defined Symbol options.

      I have to change it to following in order to have the code build.

            #elif defined STM32_SENSORTILE