AnsweredAssumed Answered

SPWF04S python over SPI

Question asked by Matteo Pezzoli on May 18, 2017
Latest reply on May 19, 2017 by Gerardo Gallucci

Hi,

I have one question about the SPWF04S module python capabilities. Looking at the "console_active" configuration variable, it seems that the python functionalities can be used only with the UART. Given that the command "AT+S.PYTHON" has its SPI equivalent though, i would say that scripts can be launched via SPI, and the only thing that needs an UART to function is the REPL; is this correct?

 

Thank you

Outcomes