AnsweredAssumed Answered

STM32F4 Temperature Function With I/O on PC6

Question asked by roofie01 on May 17, 2017
Latest reply on May 19, 2017 by waclawek.jan

Hello:

Question 1:

A question that I cannot find an answer for. If I'm using PC6 (STM32F4) as a GPIO already, can I still configure and use the internal temperature sensor on ADC16?

 

Question 2:

Using the calibration constants stored in the device, and adding some extra calibration points if required, how accurate is the temperature sensor at ranges of -40C to  +70C ?

 

Thanks...

Outcomes