AnsweredAssumed Answered

STM32 HID Multiple Endpoint

Question asked by Javier.Michael on May 14, 2017
Latest reply on May 16, 2017 by Denis M Tyurin

Hi I would like to ask if it is possible to use 2 end point for HID device?

for example: EP1 IN and out for maintenance commands/status

then EP2 IN and out for remote command and status

 

for transfer mode, i like to have the first as interrupt transfer then the other as bulk transfer..

if not possible, both interrupt transfer..

 

can anyone give me advice on this? is this feasible using generic HID driver?

 

Thanks,

Mike

Outcomes