AnsweredAssumed Answered

ST Link v2 Virtual Com Port Driver not working on Windows 10

Question asked by Nassimus Moualek on May 10, 2017
Latest reply on May 24, 2017 by Amel N

The driver STSW-LINK009 - ST-LINK, ST-LINK/V2, ST-LINK/V2-1 USB driver signed for Windows7, Windows8, Windows10 - STMicroelectronic… 

creates only the a USB serial port as shown here :

So i try to add the Virtual Port Com Manually with the action "add an old generation device" in the Device Manager

 

I try to install the STMicroelectronics\STM32 ST-LINK Utility\ST-LINK_USB_V2_1_Driver\stlink_VCP.inf

or the STMicroelectronics\Software\Virtual COM Port Driver

or the STMicroelectronics\Software\Virtual comport driver\Win8

 

Even after removing one by one, and reinstalling one at times, no one is working

 

I try all the possiblities listed in many chats or forums

 

I also attach the USBView devices listing

 

Is there a new update for the 1.4.1 VCP Driver for windows 10 ?

Outcomes