AnsweredAssumed Answered

STM32F030: Interrupt remaping to RAM

Question asked by kumar.rajeev.004 on Apr 28, 2017
Latest reply on Apr 28, 2017 by Clive One

Hi,

I am developing bootloader for STM32F030ccT6 to upgrade my Main Application through OTA. There are two application within my controller flash one is BOOTLOADER( @ 0x08000000) and other is Main Application( @ 0x08001000 ) .

Now I have done Jump from Bootloader to Application and running one 2 USART and 2 Timer Interupts of main application correctly. But here is a problem with NVIC_SystemReset and IWDG may be some other also but i checked only these two.

Actually when I reset Main Application using NVIC_SystemReset then it calls reset handler of Bootloader. But as i think it should call reset handler of Main Application rather than Bootloader.

 Please give me suggestion for this different bahaviour with NVIC_SystemReset.

Outcomes