AnsweredAssumed Answered

USB Driver Issue for Windows 10

Question asked by Kale.Sumit on Apr 27, 2017
Latest reply on Apr 28, 2017 by bhatia.kumar

Hello,

 

I am trying to integrate my custom board (STM32F205 VCT) with PC to send data over USB using Full Speed functionality.

 

Earlier i tried same with STM32F4 Discovery board & everything went right & i was able to receive data by USB over PC (Windows 10). However when i am trying to connect USB port of my custom device with PC its showing Error "USB not Detected".

 

Pin 71 is connected to D+ (White wire from USB Cable)

Pin 70 is connected to D- (Green Wire)

Ground from Custom Board

 

In Program Stack & heap Size are 0x2000 & 0x4000 resp.

 

I also read other Forums especially about Windows 10 USB Driver Issue but i coudnt figuré it out how i can solve mine

 

Do i Need to use 22ohm resistors over Pin 70 & 71 (On discovery board USB schematics its shown that 22ohm resistors are used) as USB is working over Discovery board on Windows 10 & i am able to get data over PC.

 

 

So any suggestions?

Attachments

Outcomes