AnsweredAssumed Answered

IDW01M1 Wifi Sample Codes for STM32F411RE

Question asked by Robert Kwan on Apr 26, 2017
Latest reply on Jan 28, 2018 by Duy Tran

Hello!

I recently bought the IDW01M1 WiFi expansion board 

and I am trying to have it working with the STM32F411RE.

However, from the examples in en.x-cube-wifi1_firmware.zip,

I can find the .bin file for STM32F401RE-Nucleo only

and so I tried to flash this WiFi_VCOM .bin to the STM32F411RE board.

 

I can see LED1 is green, so power is ok.

No other LED On, so module is ok?!

When I use Tera Term, I don't see any output and when I send "AT", no "OK" either.

 

So my question is that  F401RE .bin image cannot work directly on F411RE board please?!

 

Since I am still a newbie to this WiFi module, I am not sure if it will be easy to recompile the sample application for F411RE then?!

 

Any suggestion / comment is welcome.

 

 

Thanks & Best Regards,

Robert

Outcomes