AnsweredAssumed Answered

STM32F7 multi-Slave SPI with CubeMX

Question asked by David Littell on Apr 21, 2017

CubeMX 4.20.1

STM32Cube_FW_F7_V1.6.1

Target: STM32F765NIHx

 

The Reference Manual (RM0410 rev 2) Section 35.5.3 (multi-slave) Figure 390 Note 2 states that the MISO pins of all SPI Slaves must be configured as alternate-function open-drain.  However, CubeMX only offers Alternate Function Push Pull as a GPIO mode.  Is this a known problem with CubeMX meaning I'll have to manually patch the generated code?

 

Thanks,

Dave

Outcomes