AnsweredAssumed Answered

CubeMX v4.20.1 LwIP project generation for SW4STM32

Question asked by Lee.Sungjune.003 on Apr 20, 2017

Hi,

 

I'm wondering that when CubeMX generates LwIP projects, it may be pointing wrong directories for the header files. For example, it generates list of following directories:

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/lwip

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/netif

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/posix

whereas what is actually necessary is a single directory

Middlewares/Third_Party/FreeRTOS/LwIP/src/include

according to the source files. The same thing goes with

Middlewares/Third_Party/FreeRTOS/LwIP/system/arch

Middlewares/Third_Party/FreeRTOS/LwIP/system/OS

instead of

Middlewares/Third_Party/FreeRTOS/LwIP/system

I only use the .cproject file to convert it into Makefile. So I'm not 100% sure.

 

Thanks,

Outcomes