AnsweredAssumed Answered

Install firmware package from local zip file

Question asked by Zamek on Apr 19, 2017
Latest reply on May 1, 2017 by krishna K H

Hi All,

How can I install a new firmware package to stm32CubeMX. I tried to install X-NUCLEO-IDW01M1 which is a wifi driver firmware package. 

I downloaded the file (en.x-cube-wifi1_firmware.zip) and I tried to install it from cubemx, but I got an error: 

"this package version is not managed on this version of STM32CubeMX"

I use Debian Linux, and my cubemx version is: 4.20.1 STM32Cube V1.0 on help/about

The zip file is not corrupted, I can unzip it and it has a directory:

STM32CubeExpansion_WIFI1_V3.0.1 and the directory contains a package.xml file:

 

<?xml version="1.0" encoding="ISO-8859-1" standalone="no"?>
<Package DBVersion="2.0">
<PackDescription Release="FW.WIFI1.3.0.1">
<Note Release="ReleaseNotes.html"/>
</PackDescription>
</Package>

 

thx

Zamek

Outcomes