AnsweredAssumed Answered

Issue with SPI example for the STM32L432

Question asked by eddie McS on Apr 12, 2017
Latest reply on Apr 13, 2017 by eddie McS

Hi,

I have an STM32Nucleo board with the STM32L432 chip.

 

I am currently trying to get the SPI example working without success.. 

STM32Cube_FW_L4_V1.7.0\Projects\STM32L432KC-Nucleo\Examples\SPI\SPI_FullDuplex_ComPolling

 

I am using the System workbench platform to compile and build the example however when i actually run the example i see nothing(one spike sometimes) on the SPI clock line PA5 and transmission fails..

 

Has anyone successfully ran this example code before? 

 

Thanks

Ed

Outcomes