AnsweredAssumed Answered

Slave Mode Setting for DSPI1 in SPC560D40L1 Chip

Question asked by padmanabhan.preetha on Apr 11, 2017
Latest reply on Apr 12, 2017 by Erwan Y

Hi Everyone, I am using SPC560D40L1 micro controller and trying to configure DSPI1 to be in slave mode. I am using SPC5studio to make the configuration. I have set pin directions and OBE and IBE along with WPS and WPE configurations for the CS and changed directions for the clock and CS, I have made use of the CS0_1 pin as per the datasheet for enabling slave mode. Is there any other settings that i need to take care of? When i see the resgister settings of DSPI 1  during code execution it shows the channel is always in master mode. Does anyone know how i need to set the slave mode for the DSPI channel? Thanks in advance Preetha.

Outcomes