AnsweredAssumed Answered

"Internal command error" programming an STM32F072 discovery board with ST-LINK/V2

Question asked by Ishaque.Suhaib on Apr 5, 2017
Latest reply on Apr 6, 2017 by Clive One

Hello,

 

I'm trying to connect to an STM32F072R8 discovery board using an ST-LINK/V2. I am using the ST-LINK utility to do so. The utility tells me I have an "Internal command error" whenever I try to do this. Interestingly, I am able to program easily and successfully through the on-board USB programmer. I have ensured the following:

 

1) All appropriate connections are made - V_sense on VDDIO2, NRST is conencted

2) Target is externally powered

3) Flash erased (using on-board USB programmer)

4) Connect under reset mode 

5) Attempted many different SWD frequencies (4 MHz to 5 kHz)

6) Updated the ST-LINK firmware. 

 

I have attached a photo of my connections to between the ST-LINK and dev board. I have also attached the trace log output file when I try to connect with an SWD frequency of 100 kHz. I have also attached a screenshot of my settings. 

 

I have searched the internet for other potential fixes, but I can't find anything. I greatly appreciate any help in debugging this issue! Thank you.

Outcomes