AnsweredAssumed Answered

Problem in loading .hex and .bin file

Question asked by Santhamurthy R on Mar 24, 2017
Latest reply on Mar 24, 2017 by Erwan Y

Hello All,

 

I am using SPC560B54L5 Discovery board(SPC560B-Discovery), SPC5studio version 5.2.3 and UDE Visual Platform 4.2 version.

 

When I  try to load the application the .elf is working fine. If i try to make use of .hex or .bin file (as per my requirement)

I am facing following problems,

 

When I try to load ".hex" file the code gets loaded successfully but while running it is throwing an error as " Unknown Break cause". Similarly, when I try to even  load ".bin" file it prompts with "Unknown File Format" error.

 

Error While loading .hex file:

 

 

 

 

Error While loading .bin file:

 

Kindly suggest if I need to do the changes to the settings or preferences in IDE (or) UDE

 

Regards,

R.santhamurthy

Outcomes