AnsweredAssumed Answered

Spriti1 application

Question asked by abimbola.idris on Mar 23, 2017

Hello everybody,

I have the STEVAL-IKR001Vx evaluation kit and the SDK-2.0.1 and SDK-2.2.0. I have been trying to work with the GenericBasic_A and B. Both files compiled without any error in IAR and Keil v4. However, nothing was happening after downloading the firmware onto the board as indicated in the readme.txt. I noticed that the whole SDK was configured for three evaluation kits (STEVAL-IKR001Vx, STEVAL-IDS001Vx and STEVAL-IKR001Vx). Do I need to specify the type of evaluation board before performing the compilation? if yes, where can I do that?

 

Thanks.

Outcomes