AnsweredAssumed Answered

Bug report Cube+FreeRTOS

Question asked by Osto on Sep 7, 2014
Latest reply on Sep 26, 2014 by Osto
There is a bug in STM32Cube (newest version). When I use FreeRTOS then the eTaskGetState() is not available. In FreeRTOS.h which is generated by Cube, the variable INCLUDE_eTaskGetState is set to 0 which means dont include it,

There is no value I can enable in Cube which results in setting INCLUDE_eTaskGetState to 1.
In addition to that when I set this variable to 1 by myself then the value is overwritten next time I generate the project.

Outcomes