AnsweredAssumed Answered

LSM6DSL Min/Max specifications for ODR (Output Data Rate)

Question asked by Niclaes.Christophe on Mar 21, 2017
Latest reply on Apr 9, 2017 by Miroslav B

I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as "Typical". Could I get a more precise specification for the ODR, e.g. min/max values over the entire temperature range. I suppose this ODR is generated from an internal oscillator with tolerance, temperature drift, ...

Outcomes