AnsweredAssumed Answered

No interrupt on tmr overflow

Question asked by John Hite on Mar 20, 2017
Latest reply on Mar 20, 2017 by Clive One

STM32F437

 

I am using TIM4 for input capture and an interrupt occurs when external events occur. However I stopped the external event and no interrupt occurs on overflow although the UIF bit is set in SR. Code snippet below and TIM4 is listed below that.

 

Thank you,

JH

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

void RpmTask(void *p_arg)
{
  TIM_TypeDef *tim4 = TIM4;
  RCC_TypeDef *rcc = RCC;
  OS_ERR err;
  uint16_t rpm4 = 0;

 

  NVIC_InitTypeDef NVIC_InitStruct;
  /*Interrupt packet initialization*/
  NVIC_InitStruct.NVIC_IRQChannel = TIM4_IRQn;
  NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1;
  NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0;
  NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStruct);
 
  //RPM timer setups
  // APB1PeriphClock - 42 MHz
  // APB2PeriphClock - 84 MHz
  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3 | RCC_APB1Periph_TIM4, ENABLE);
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_TIM9, ENABLE);

 

  TIM_TimeBaseInitTypeDef tim4_base;
  tim4_base.TIM_Period = 0xFFFF;
  tim4_base.TIM_Prescaler = 0; //42000 -1;
  tim4_base.TIM_ClockDivision = TIM_CKD_DIV1;  //digital filter clk div, don't care, filtering is off
  tim4_base.TIM_CounterMode = TIM_CounterMode_Up;
  tim4_base.TIM_RepetitionCounter = 0; //t1&t8 pwm, don't care
  TIM_TimeBaseInit(TIM4, &tim4_base);

 

  TIM_ICInitTypeDef tim4_icInit;
  tim4_icInit.TIM_Channel = TIM_Channel_1;
  tim4_icInit.TIM_ICPolarity = TIM_ICPolarity_Rising; //r, f, both
  tim4_icInit.TIM_ICSelection = TIM_ICSelection_DirectTI; //dir, ind, trc
  tim4_icInit.TIM_ICPrescaler = TIM_ICPSC_DIV1; //1-8
  tim4_icInit.TIM_ICFilter = 0x0;
  TIM_ICInit(TIM4, &tim4_icInit);
 
  TIM_UpdateDisableConfig(TIM4, 0);
    
  /* Enable the CC2 Interrupt Request */
  TIM_ITConfig(TIM4, TIM_IT_CC1, ENABLE);

 

  /* TIM enable counter */
  TIM_Cmd(TIM4, ENABLE);

 

  uint16_t cnt = 0;
  while(1)
  {
    cnt = TIM_GetCounter(TIM4);
    OSTimeDlyHMSM(0u, 0u, 0u, 1000u, OS_OPT_TIME_HMSM_NON_STRICT, &err);
  }
}

 

void timer4_isr(void)
{
  volatile int optimizerBlock = 0;
  TIM_TypeDef *tim44 = TIM4;
  uint16_t rpm4 = 0;
  uint32_t cnt;
  CPU_SR_ALLOC();
 
  CPU_INT_DIS();
  OSIntNestingCtr++;
  CPU_INT_EN();
 
  if (TIM_GetITStatus(TIM4, TIM_IT_Update) == SET)
  {
    ...
     TIM_ClearITPendingBit(TIM4, TIM_IT_Update);
  }
 
 
  if (TIM_GetITStatus(TIM4, TIM_IT_CC1) == SET)
  {
    ...
   TIM_ClearITPendingBit(TIM4, TIM_IT_CC1);
  }
 
  OSIntExit();
}

 


Expression    Value    Location    Type    
tim4    0x40000800    R5    TIM_TypeDef *    
CR1    0x0001        
RESERVED0    
CR2    0x0000        
RESERVED1    
SMCR    0x0000    
RESERVED2    
DIER    0x0002    
RESERVED3    
SR    0x001D        
RESERVED4    
EGR    0x0000        
RESERVED5    
CCMR1 0x0001    
RESERVED6    
CCMR2 0x0000    
RESERVED7    
CCER    0x0001    
RESERVED8    
CNT    51557        
PSC    0x0000        
RESERVED9    
ARR    0x0000FFF
RCR    0x0000        
RESERVED10    
CCR1    0x00000000        
CCR2    0x00000000        
CCR3    0x00000000        
CCR4    0x00000000        
BDTR    0x0000    
RESERVED11    0x0000    
DCR    0x0000    0x40000848
RESERVED12    0x0000            
DMAR    0x0001    0x4000084C    
RESERVED13    0x0000            
OR    0x0000    0x40000850        
RESERVED14    0x0000            

Outcomes