AnsweredAssumed Answered

X-NUCLEO_CCA02M1

Question asked by Daniel Martinez Martinez on Mar 19, 2017
Latest reply on Apr 25, 2017 by Daniel Martinez Martinez

Hello all,

 

I have bought a NUCLEO-L476RG board and a X-NUCELO_CCA02M1 board a couple of months ago and I have flashed the stm32f476RG micro of the board with the sample application that it is include in the folder

...\Projects\Multi\Applications\Microphones_Streaming\Binary\STM32L476RG-Nucleo\MicrophonesStreaming_2Channels_16KHz.bin

and it works the application with Audacity. It is possible to record with the board and much more. To make it works, I had also to change the bridges of the CCA02M1 board according to the UM1900 User manual section 3.4.2.1  Jumper settings for DFSDM-based systems for 1 or 2 microphone acquisition.

 

..\Projects\Multi\Applications\Microphones_Streaming\Binary\STM32L476RG-Nucleo\MicrophonesStreaming_2Channels_16KHz.bin

 

But the fact is, when I open the project with SystemWorkbench that is here ..\Projects\Multi\Applications\Microphones_Streaming\SW4STM32\STM32L476RG-Nucleo\STM32L476RG-MEMSMIC1

and I compile and debug or run the program on the board it does not works the application with Audacity.

 

In the documentation says very clear this:

 

@par Hardware and Software environment

 

  - This example runs on STM32F401RE, STM32F072RB, STM32L053R8, STM32L476RG and STM32746ZG devices.
    
  - This example has been tested with STMicroelectronics STM32F401-Nucleo,
    STM32L476-Nucleo, STM32L053-Nucleo, STM32F746-Nucleo-144 and STM32F072-Nucleo
    boards and can be easily tailored to any other supported device
    and development board.

 

Maybe somebody change something in the some file and it didn't test it.

 

To buy something and then it doesn't go it is not fair play.

 

Here I put the links of the boards

 

NUCLEO-L476RG - STM32 Nucleo-64 development board with STM32L476RG MCU, supports Arduino and ST morpho connectivity - ST… 

 

http://www.st.com/en/ecosystems/x-nucleo-cca02m1.html 

 

I hope to hear from you soon.

Bye

Outcomes