AnsweredAssumed Answered

Is the DCMI capable of acquiring 12-bit raw bayer image data?

Question asked by M. Jeong on Mar 12, 2017
Latest reply on Mar 12, 2017 by Clive One

The data sheet of the STM32F429 shows that its camera interface can take 14-bit parallel data and the maximum data rate is 54MB/s. Also it says the interface supports 8-bit progressive video monochrome or raw bayer format, without mentioning higher bitdepth. I wonder if it does imply that you can't capture 10-bit or 12-bit raw bayer image data with the DCMI.

Outcomes