AnsweredAssumed Answered

How to communicate two microcontrollers to a single pc via ethernet tcp/ip

Question asked by talvar.sulochana on Mar 10, 2017
Latest reply on Mar 13, 2017 by talvar.sulochana

Hi,

 

The communication between single microcontroller and pc is works fine through ethernet tcp/ip . problem occurs only when i connect two microcontroller to a single pc via ethenet cable,Here d-link 5-port 10/100 desktop is used for multiple connection.when connection made for multiple microcontroller ,the communication doesn't work properly.Either one connection will be in active condition other will be inactive.

 

I need solution to overcome this issue.My requirment is from pc it sends query to microcontroller-1 after receiving response from microcontroller-1 .It has send next query to Microcontroller-2.Process should be repeat.

 

Is it possible? If yes please please guide me. Please anyone reply as soon as possible......

 

Thanking You....

Outcomes