AnsweredAssumed Answered

STM32F030K6T6 does not have usart library . what should i do?where to find its library?

Question asked by navid ansari on Mar 8, 2017
Latest reply on Mar 8, 2017 by Clive One

hi

first i look here

but there is no usart driver.

this is my schematic

according to schematic i use pa2 and pa3 as usart.

please tell me if there is any library to init usart and use it.

if there is not .

datasheet give me something but its hard to understand . what to do?

first  Alternate function selection

/* This sequence select AF2 for GPIOA5, 8 and 9. This can be easily adapted
with another port by changing all GPIOA references by another GPIO port,
and the alternate function number can be changed by replacing 0x02 for
each pin by the targeted alternate function in the 2 last code lines. */

/* (1) Enable the peripheral clock of GPIOA */
/* (2) Select alternate function mode on GPIOA pin 5, 8 and 9 */
/* (3) Select AF2 on PA5 in AFRL for TIM2_CH1 */
/* (4) Select AF2 on PA8 and PA9 in AFRH for TIM1_CH1 and TIM1_CH2 */
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; /* (1) */
GPIOA->MODER = (GPIOA->MODER & ~(GPIO_MODER_MODER5 | GPIO_MODER_MODER8
| GPIO_MODER_MODER9)) | GPIO_MODER_MODER5_1
| GPIO_MODER_MODER8_1 | GPIO_MODER_MODER9_1; /* (2) */
GPIOA->AFR[0] |= 0x02 << (5 * 4); /* (3) */
GPIOA->AFR[1] |= 0x02 | (0x02 << ((9 - 8) * 4)); /* (4) */

but line 3 and line 4 is so hard to get . why 5*4 why ((9-8)*4)) :!

 

please somebody help me

Outcomes