AnsweredAssumed Answered

SHA256 RSA digest

Question asked by Pawlyk.James on Mar 1, 2017
Latest reply on Mar 2, 2017 by Clive One

I have this working on a stmicroF427 part and I am trying to run the same code on a STmicroF103.  The only changes are that I used the M3 versions of the library on the F103 part, and the 427 system uses cube and the HAL libraries.  The code running on the 103 does not generate a correct digest.  I have verified that the data is good (there is a CRC also).  Can someone verify that this does work on the F103 part and that there are no setup steps that I may need to do to run this?

Outcomes