AnsweredAssumed Answered

CubeMX bug on STM32F4 ADC config?

Question asked by Andres Cao on Mar 1, 2017
Latest reply on May 9, 2017 by Jeanne Joly

Hi guys!

 

I'm currently using the Nucleo 64 board with the STM32F446RE chip.

 

This microcontroller has 3 ADCs, which according to the reference manual (see pic), can be configured to run as ADC1+ADC in simultaneous mode, and ADC3 independently. This would be for my configuration, MULTI = 0b00110.

 

In this way I can use the ADC1+ADC2 to simultaneously sample current, and do other stuff with ADC3.

 

However, in CubeMX when I select Mode as "Dual Regular Simultaneous Only", ADC3 gets locked up in that same configuration (see pic).

 

Unless I misunderstood the Reference Manual, something would seem to be wrong.

 

Any clues?

Outcomes