AnsweredAssumed Answered

STM32L031 program does not run.

Question asked by Mads Enevoldsen on Feb 28, 2017
Latest reply on Mar 2, 2017 by Mads Enevoldsen

1:

I have developed a small program for the STM32L031 Nucleo-32 using the example UART_TwoBoards_ComIT. The program run on the STM32L031 Nucleo-32 develop-board. When I load* the program to our own HW it does not start, I have tried with and without the compiler directive USE_STM32L0XX_NUCLEO_32. I suspect the system clock generation, but can’t find where it is setup.

*I load the program using STM flash_loader_demo_v2.8.0.

 

2:

I want to use the ST-LINK V2 for debug should the data port be connected to PA13?

 

Do any have a hint or comments that could help me?

-Mads

Outcomes