AnsweredAssumed Answered

unable to flash the development SPC560B-Dis

Question asked by raj.nishil on Feb 28, 2017
Latest reply on Mar 9, 2017 by Erwan Y

Hi All,

Appreciate your time and help.

i am using the SPC560B-DIS development board with the spc5studio IDE.

all of a sudden when i tried to flash the development board i got an error in the log saying : Error, Core::PpcJtagTargIntf, Connection to target lost !
i suspected a loose cable to be the culprit but then the same cable works perfectly fine with the other EVM(evaluation board).
Then i also checked the mini usb power/debug female port connector on the board which is fine as well.(did not see any physical damage on it attached is the image below).

i have attached my boards log file from the UDE when i got the board connection lost error.

Outcomes