AnsweredAssumed Answered

STM32 with USB Host and SD Card Interface

Question asked by Nimit Vachhani on Feb 27, 2017
Latest reply on Feb 27, 2017 by Maxime TEISSIER

Greetings to all the GEEKS.

 

Well i am looking for STM32 microcontroller that has usb host capability as well as it can interface with micro sd card or sd card. The reason for usb host capability is --- I want to store the data on to usb pen drive that is fat or fat32 formatted. I want the interface with micro sd card or sd card for the same reason. If usb pen drive is not attached then i want to store data on to micro sd card or sd card.

 

Any advice will be helpful. I don't mind the usb host speed i.e. i am okay if i don't get usb host capability on full speed.

Outcomes