AnsweredAssumed Answered

Infrared contol

Question asked by bibari.wael on Feb 13, 2012
Latest reply on Feb 15, 2012 by Billino
hello,
I want to control an Infrared system. with the USB-UIRT I could extract the Pronto Remote code and I have to pass through a microcontroller and an IR LED.
the signal frequency is 37.7 kHz.
the frame is:
0000 006D 0000 0074 0070 0157 0013 003C 0013 0015 0013 0015 0013 0015 0013 0016 0013 0015 0013 0015 0013 0015 0013 0017 0015 003B 0013 0016 0012 0016 0014 003C 0013 003B 0013 003C 0013 0015 0013 003 C 0013 003B 0013 003B 0013 003C 0013 0016 0014 0016 0012 0015 0013 0015 0013 0015 0013 0016 0012 0015 0013 0015 0013 0015 0013 0017 0014 0015 0013 0015 0013 0015 0013 0016 0013 0015 0013 0015 0013 0013 003C 003C 003C 0015 0012 0017 0014 0015 0013 0015 0013 0015 0013 0016 0013 0015 0013 003C 0013 0015 0013 003C 0015 0015 0013 003 E 0014 0015 0013 0015 0013 0015 0013 0015 0013 0015 0013 0015 0012 0045 0070 0158 0013 003B 0013 0015 0013 0015 0013 0015 0013 0015 0013 0015 0013 0016 0013 0015 0013 0015 0013 003C 0013 0015 0013 0015 0013 0015 0013 0016 0013 003B 0013 003C 0013 0015 0013 003 D 0014 003B 0013 003B 0013 003B 0013 003C 0013 003B 0013 003C 0013 003C 0012 0015 0013 0016 0014 0015 0013 003 D 0015 003C 0013 003B 0013 0015 0013 003 B 0013 003D 0014 0016 0012 0015 0013 0015 0013 0015 0013 0016 003B 003D 0013 0013 0015 0015 0013 0013 0016 0014 003 B 003 C 0013 003C 0012 0015 0013 0015 0013 0015 0013 0016 0012 0017 0015 0015 0013 0015 0013 0015 0013 0014 003B 003B 0011 0F76


the LED is connected to a pin I / O of the microcontroller.

I have to convert this code to send it and the receiver can receive the frame, decode and execute the command OFF.
I await your suggestions.

Outcomes