AnsweredAssumed Answered

STM3210E-EVAL dual motor drive

Question asked by reichert.sebastian on Feb 8, 2012
Latest reply on Feb 23, 2012 by reichert.sebastian
Hallo,

is it possible to drive two motors with this eval board? I don't want to drive them simultaneously and independently but "mutual exclusive", i.e. I have one enable signal for every motor, while only one is true at a time. On the uC only one control function is running at any time.
Just using a Y-cable from the MC connector to two power stages wouldn't work, as I have no possibility to disable one of the two motors, right?

On the other hand, is it possible to connect some GPIOs to a second power stage to do real dual drive simultaneously? (This would be some kind of a second MC connector which doesnt exist on my board).

thanks in advance.

regards,
sebastian

Outcomes