AnsweredAssumed Answered

Unable to set Port and Pin in Motor Control Workbench for OverCurrent Protection Disable.

Question asked by ericc on Dec 29, 2011
Latest reply on Jan 2, 2012 by Gigi
[Resolved]: When the Over-current protection disabling network check box is clicked on the (Power Stage - Over Current Protection) page the port and pin values can then be changed.

-----------------------------------------------------------------------------------------------

I am unable to change the port and pin for the Over current Protection Disable in Motor control workbench.  All the enables for this are set properly.  I can edit the output files and change the pin but not in the MCWB application.  Is this a bug or am I missing something? 

Photo included shows option greyed out.  
OCProt.JPG

-------------------------------------------------------------------------------------------------
Secondly When I enable the ICL Shutout option I get a warning saying : "feature not supported by default STM32 PMSM FOC FW library"

How do I enable this feature?

Eric

Outcomes