AnsweredAssumed Answered

Trouble connecting to a network (SPWF01SA module)

Question asked by Matteo Pezzoli on Feb 23, 2017
Latest reply on Mar 1, 2017 by Gerardo Gallucci

Hi,

Using the SPWF01SA module, i managed to connect to all of the networks i found here, except one. I probably got the configuration wrong, but i can't find where's the error. To my knoweledge, the only difference this network has from the other networks (to which i can succesfuly connect) is that it gives out ips in the 10.20.0.x range, instead of the usual 192.168.0.x one.

I tried disabling the dhcp and assigning the gateway ip and dns ip manually, also setting a static ip (i used 10.20.50 or something like that), to no avail.

I should also mention that both my laptop and phone can connect to this network without problem.

 

Here's the configuration i am using:

# Dumping All Configuration Keys:
#  nv_manuf = ST
#  nv_model = SPWF01SA1
#  nv_serial = 3514D04763
#  nv_wifi_macaddr = 00:80:E1:B4:7D:1F
#  blink_led = 0
#  wind_off_low = 0x00000000
#  wind_off_medium = 0x00000000
#  wind_off_high = 0x00000000
#  user_desc = anonymous
#  escape_seq = at+s.
#  localecho1 = 0
#  console1_speed = 115200
#  console1_hwfc = 0
#  console1_enabled = 1
#  sleep_enabled = 0
#  standby_enabled = 0
#  standby_time = 10
#  wifi_tx_msdu_lifetime = 0
#  wifi_rx_msdu_lifetime = 0
#  wifi_operational_mode = 0x00000011
#  wifi_beacon_wakeup = 1
#  wifi_beacon_interval = 100
#  wifi_listen_interval = 0
#  wifi_rts_threshold = 3000
#  wifi_ssid = 53:4D:45:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
#  wifi_ssid_len = 3
#  wifi_channelnum = 6
#  wifi_opr_rate_mask = 0x00003FCF
#  wifi_bas_rate_mask = 0x0000000F
#  wifi_mode = 1
#  wifi_auth_type = 0
#  wifi_atim_window = 0
#  wifi_powersave = 0
#  wifi_tx_power = 18
#  wifi_rssi_thresh = 0
#  wifi_rssi_hyst = 0
#  wifi_ap_idle_timeout = 120
#  wifi_beacon_loss_thresh = 10
#  wifi_priv_mode = 2
#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00
#  wifi_wep_key_lens = 00:00:00:00
#  wifi_wep_default_key = 0
#  wifi_wpa_psk_raw = 34:2D:CC:99:D8:94:02:46:75:25:75:E2:E9:6D:F9:5C:AF:C5:A8:B2:F3:26:7C:4E:4F:14:67:2A:88:F9:09:85
#  wifi_wpa_psk_text = ywifi_sap
#  ip_use_dhcp = 1
#  ip_use_httpd = 1
#  ip_mtu = 1500
#  ip_hostname = iwm-B4-7D-1F
#  ip_apdomainname = captiveportal.net
#  ip_ipaddr = 192.168.0.50
#  ip_netmask = 255.255.255.0
#  ip_gw = 192.168.0.1
#  ip_dns = 192.168.0.1
#  ip_http_get_recv_timeout = 3000
#  ip_dhcp_timeout = 20
#  ip_sockd_timeout = 250

 

OK

 

Thank you

Matteo

Outcomes