AnsweredAssumed Answered

BlueNRG-ms doesnt follow Bluetooth core specification?

Question asked by Paulstrom.Bjorn on Feb 21, 2017
Latest reply on Feb 22, 2017 by Paulstrom.Bjorn

Hello, I am using a BlueNRG-ms (IDB05A1) flashed to latest fw 7.2c trying to develop a HID compliant mouse for Windows.

 

However when pairing with windows using only the basic GATT and GAP(no other services or changes) from the BlueNRG GUI there are some problems, Windows says:

 

Device (0x280E1003C2A) is not Compliant with the Bluetooth Core Specification: previous attribute was a (Characteristic), current attribute is a (Descriptor).

 

Is this a bug or is Windows wrong? BlueNRG-ms page states:

"The BlueNRG-MS is a very low power Bluetooth low energy (BLE) single-mode network processor, compliant with Bluetooth specification v4.1."

 

Is this a cause for concern?

Outcomes