AnsweredAssumed Answered

FR_NO_FILESYSTEM ,FatFs,4-pins SDcard with Nucleo-L476RG

Question asked by Anna on Feb 22, 2017
Latest reply on May 22, 2018 by Manjesh R

Hey all,

I want to write to SD card, I'm Using cube-mx stm32 Nucleo-L476RG MCU ,and 4-pin SD card, 

I attach my cube project, the main program has the following code:

 

declaring and init :

FATFS SDFatFs;
FIL MyFile;
extern char SD_Path[4]; /* SD logical drive path */
/* USER CODE END 0 */

int main(void)
{

/* USER CODE BEGIN 1 */
FRESULT res;
uint32_t byteswriten,byteread;
uint8_t wtext[]="Hello from STM32!!\0";
/* USER CODE END 1 */

/* MCU Configuration----------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();

/* Configure the system clock */
SystemClock_Config();

/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_DFSDM1_Init();
MX_SDMMC1_SD_Init();
MX_FATFS_Init();
MX_TIM6_Init();

MX_SDMMC1_SD_Init();

 

 

 

I am trying to write to sd card by the following code:

 

if(res=f_mount(&SDFatFs,(TCHAR const*)SD_Path,0)!=FR_OK)
{
Error_Handler();
}
else
{

if(res=f_open(&MyFile,"0:/mywrite.txt",FA_CREATE_ALWAYS | FA_WRITE ) != FR_OK)
{
Error_Handler();
}
else
{
res=f_write(&MyFile,wtext,sizeof(wtext),(void*)&byteswriten);
if((byteswriten==0) || (res!=FR_OK))
{
Error_Handler();
}
else
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}

f_close(&MyFile);
}
}

I get FR_NO_FILESYSTEM if the SD is connected and if the SD is not connected, I get FR_NOT_READY,

Thanks for any help.

Outcomes