AnsweredAssumed Answered

STM32F769I-DISCO printf() using ITM/SWO

Question asked by dake.dheeraj on Feb 21, 2017
Latest reply on Sep 1, 2017 by simoes.jose

Hello everyone,

I am trying to redirect printf() to ITM using the tutorial in here and view the output. I followed the steps as shown in that video but I was unable to see the output because I have a FREE version. I noticed that STM32 ST-LINK utility software also has SWV option. So I tried the following.

 

1. ST-LINK firmware update (successful)

2. Target connect (successful)

3. Clicked SWV icon

4. Entered 216 MHz in System clock and stimulus port is set to 0

5. Clicked start

I can't see any output here.

 

My project cubeMX configuration is as follows:

SYS is configured as Trace Asynchronous SW. The rest of the pins are in default state. I am using printf() to print output. 

 

I connected my board via ST-LINK USB port to my computer. How do I see the printf() output?

 

I also tried to define a _write function main.c and calling printf() as described in 10_Complementary debug tools - printf.pdf in STM material\USER_MATERIAL\Slides but that didn't help either. Any ideas on how to get this ITM work?

Outcomes