AnsweredAssumed Answered

Compiled HAL Library Errors

Question asked by baird.hal.001 on Feb 20, 2017
Latest reply on Feb 20, 2017 by baird.hal.001

Ever since the dawn of HAL, every HAL library I have tried has contained compiler detected errors. My latest frustration source is the STM32L4xx HAL library version 1.6.0. The problems are diverse and include:

  1.         Typo differences in peripheral register bit definitions between the reference manual, the device stm32l4yyxx.h file and  the hal peripheral .c file (yy = 76, 86, etc.).
  2.         Missing peripheral register bit definitions in the device stm32lyyxx.h file.
  3.         Hal peripheral .c file with a code segment with no conditional compile referencing a conditionally compiled parameter.

Some of the problems I can fix myself, but I don’t think I should have to. The root problem seems to be incomplete or non-existent library compile and fix before release.

 

It’s tough to get universal HAL acceptance with stuff like this going on.

Hal

Outcomes