AnsweredAssumed Answered

STM32F4 Camera with STM32F7 Discovery board?

Question asked by Cachan.Xav on Feb 19, 2017
Latest reply on Apr 21, 2017 by Korzha.Alex

Hi all,

I'm trying to use the camera STM32F4DIS-CAM with my STM32F7 Discovery board, with Keil uVision IDE. I have downloaded STM32Cube, and in the examples there is a BSP directory, with BSP drivers examples, including a camera.c for the camera. All the drivers are working well (LCD, Touchscreen, audio, sram...), but the programm stops when the Camera example starts. It seems that the initialization is OK, I can see "QQVGA camera stream", but then nothing happens, the stream is only a white screen, and the touch actions do not work (change brighness, contrast...). The "user button" also do not work anymore...

Do you have an idea of the way I should follow to solve such problem?

Thank you.

Best regards,

Outcomes