AnsweredAssumed Answered

FW problems with the X-Nucleo-IDW01M01

Question asked by Paolo Nogara on Feb 17, 2017

Hello everyone,
I'm starting to use the shield X-Nucleo-IDW01M01 with a Nucleo F401RE and I have some problem with the FW update. I follow the guide "X-NUCLEO-IDW01M1- FW upgrading over UART_v1.1" but at the end I only see the message loaded from the Nucleo but I don't see activities by the shield (see "test.jpg).

In particular, the only LED that lights up is the LED1. The yellow LED on the shield lights up only when I try to load the example bin file "WiFi_VCOM".
I hope for your help, greetings