AnsweredAssumed Answered

STM32 Time base Interrupt

Question asked by W.A on Feb 16, 2017
Latest reply on Feb 21, 2017 by W.A

Hi,

I need Help regarding time base.

I found one of the example and tried to modify that for STM32 F4 Discovery board.

I want to count number of external pulses by using TIM4 in 1.13 ms. So the time base is configured to generate interrupt after each 1.13 ms (as the read_me file states). the code is generating interrupt but it is not after 1.13 ms. can any body help me in this matter. I have attached the files for your review. 

 

Thanks in Advance  

Outcomes