AnsweredAssumed Answered

Timer in TIM_OCMODE_ACTIVE is always HIGH

Question asked by smrtkai on 15-Feb-2017
Latest reply on 20-Feb-2017 by waclawek.jan

Hi,

 

I want to generate a square wave using Timer mode TIM_OCMODE_ACTIVE. I have generated the code using STM32CubeMX and I am using a STM32F429I Discovery Board.

 

The output pin is always "HIGH". For TIM_OCMODE_INACTIVE the pin is always "LOW".

 

Changing to TIM_OCMODE_TOGGLE the ouput pin changes states. I am expecting changes on the output pin for the other modes as well. What am I doing wrong in the other modes? My configuration looks like this.

 

Thanks in advance.

 

 

void MX_TIM1_Init(void)
{
  TIM_MasterConfigTypeDef sMasterConfig;
  TIM_OC_InitTypeDef sConfigOC;
  TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig;

  htim1.Instance = TIM1;
  htim1.Init.Prescaler = 10;
  htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim1.Init.Period = 10;
  htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim1.Init.RepetitionCounter = 0;
  if (HAL_TIM_OC_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }

  sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }

  sConfigOC.OCMode = TIM_OCMODE_ACTIVE;
  sConfigOC.Pulse = 0;
  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
  sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
  sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
  sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
  if (HAL_TIM_OC_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
  {
    Error_Handler();
  }

  ...

}

Outcomes