AnsweredAssumed Answered

BlueNRG-MS connection interval

Question asked by Comotti.Daniele.001 on Feb 14, 2017
Latest reply on Feb 15, 2017 by Antonio Vilei

Hi,

I'm using the BlueNRG-MS chipset. As far as I've understood, the connection interval is set through "aci_gap_set_discoverable" and if the related arguments of the function (SlaveConnIntervMin and SlaveConnIntervMax) are 0, it is set to 7.5 ms (as for BLE standard), otherwise it is set using multiples of 1.25 ms. Which is the minimum value which can be set? Can the connection interval be set to 1.25 ms in order to maximize throughput?

 

Thank you,

Daniele

Outcomes