AnsweredAssumed Answered

SWT interrupt

Question asked by vierman.gert on Feb 9, 2017
Latest reply on Feb 9, 2017 by vierman.gert

Hi,

 

I'm having problems with the SWT generating an interrupt before going through reset on the SPC560P44L3

 

ITR bit is enabled, and when I trigger the watchdog I see the TIF bit switch on after the first timeout, and after the second timeout the CPU is reset, as expected.

 

Vector28 is not called when TIF goes active, however. Do I need to configure anything else in addition to the ITR bit to get this to work?

 

Thanks,

Outcomes