AnsweredAssumed Answered

When enable USBHS internal IP DMA, STM32F746 discovery board fail to enumerate. 

Question asked by HU.HUI on Feb 8, 2017
Latest reply on Apr 28, 2017 by Vito Marolda

I use STM32CubeMX to generate STM32F46 discovery board project, just enable "USBHS internal IP DMA",  Choose CDC class, show as the attached picture 01, when I compile and run the firmware, connect the USB HS port, I use the USBView.exe from win10 to check the USB information, it shows "FailedEnumeration", show as the pitcture02. If I disable "USBHS internal IP DMA", then everything will be fine. Can anybody tell me how use the USBHS internal IP DMA?Is any other setting I should do? Thanks!

Attachments

Outcomes